Step Trigger
This is a source sequence parameter which specifies how the source step is to be triggered. The choices are:
- IMMediate (equivalent to Free Run); the source begins generating a waveform without waiting for a
trigger.
- INTernal; the source step is triggered from the test set’s analyzer.
- KEY
- BUS
- EXTernal2; the source step is triggered from the TRIGGER 2 IN port on the rear panel of the test set.